Key takeaways:

  • Predictive maintenance helps healthcare facilities identify equipment degradation before failures compromise patient safety, disrupt critical environments or create compliance risks with violations and fines.
  • Healthcare facilities can use condition-based, predictive approaches to guide maintenance with real-time equipment data.
  • OpenBlue Equipment Performance continuouorly monitors data from more than 130 ensbuilding sources to centralize equipment health, performance trends and emerging risks.
  • Infrastructure upgrades and OpenBlue helped one healthcare campus cut natural gas use by 69% and generate about $870,000 in annual savings.
  • At another hospital, integrated smart systems helped save approximately 600 preventive maintenance hours annually and about 4,000 troubleshooting hours during the first year.

Healthcare facilities operate some of the most demanding environments in the built world, where even minor system disruptions can affect patient care, compliance and revenue. As staffing pressures increase and building systems become more complex, healthcare organizations are turning to predictive maintenance to reduce operational risk and improve resilience.

Clinical operations continue around the clock, while ventilation, air pressure, temperature and humidity must remain within precise parameters across critical spaces like operating and isolation rooms. A system interruption not only delays procedures and disrupts patient care, but it also creates compliance risks and reduces revenue.

For facility operators and healthcare operations leaders, the challenge is preventing downtime while improving response times. Learn how predictive maintenance can support 24/7 operations with greater precision, consistency and resilience.

The maintenance maturity spectrum: From reactive to predictive

Healthcare facilities are moving beyond traditional maintenance models as AI expands what teams can monitor, analyze and act on, with 65% of healthcare facility managers already using AI to improve facility operations.

Selecting the right solutions requires a clear understanding of the maintenance maturity spectrum, including how each approach differs in intervention timing, operational visibility and system-wide coordination.

  • Traditional preventive maintenance (calendar-based): Schedules services at fixed intervals, regardless of an asset’s condition or utilization. While it prevents some unexpected failures, it may also result in servicing healthy equipment while missing early signs of degradation between inspections. Calendar-based schedules can't easily adapt to actual performance or changing demands in a 24/7 hospital environment.
  • Condition-based maintenance (threshold-based): Triggers service when monitoring detects that equipment degradation has reached a predetermined threshold. It gives teams more visibility, but action occurs only after warnings appear, often overlooking system interdependencies or ideal intervention times.
  • Predictive and prescriptive maintenance (AI-driven): Uses AI-powered fault detection and diagnostics to continuously assess equipment health, recognize degradation patterns and recommend action based on real-time condition and utilization. OpenBlue applies predictive maintenance intelligence across connected building systems, helping teams intervene early enough to prevent failure without unnecessarily servicing equipment. It can also support maintenance cost control and repair-versus-replace decisions.

At Cortellucci Vaughan Hospital in Canada, OpenBlue and Metasys enabled continuous HVAC monitoring, real-time alerts and faster fault identification. The hospital saved 600 hours annually on preventive maintenance and 4,000 hours of troubleshooting during its first year and maintained required temperature and humidity levels in critical areas, reducing the potential for compliance issues and risks to human health.

See how healthcare facilities are turning complexity into strategic advantage

Watch webinar

Challenges and benefits in healthcare environments

Healthcare facilities must maintain precise environmental conditions while keeping complex building systems running continuously. Predictive maintenance helps teams manage these competing demands by connecting equipment data, operational priorities and maintenance workflows across the facility.

The challenge: Precision environmental controls and system interdependencies

Per ASHRAE Standard 170, healthcare HVAC systems must meet strict requirements for air changes, pressure, temperature and humidity across 60+ space types to prevent airborne contamination and surgical site infections. Failing to comply with The Joint Commission’s EC.02.05.01 standards risks regulatory penalties or loss of Medicare and Medicaid reimbursement from not satisfying the CMS Conditions of Participation.

Because hospitals operate 24/7, there are no low-risk maintenance windows. Unplanned failures lead to delayed procedures, emergency repair costs, revenue loss and reputational risk. Predictive maintenance solves this by identifying emerging issues earlier, allowing teams to plan interventions deliberately and document conditions for audit readiness.

The solution: From alarms to unified building intelligence

Many healthcare facilities already use sensors, dashboards and fault detection tools, but facility managers are left having to manually balance several factors, including:

  • HVAC alerts
  • Operating room schedules
  • Energy constraints
  • Compliance requirements
  • Competing maintenance priorities

OpenBlue transforms raw, disparate building data from equipment, controls, alarms and maintenance systems into actionable operational insight. By combining continuous monitoring with AI-driven analysis, the platform identifies patterns, ranks issues by operational impact and surfaces the actions that matter most.

From there, OpenBlue coordinates the response through automated work orders and real-time setpoint adjustments. Integrating seamlessly with existing BMS and CMMS infrastructure, it gives facility teams a single, unified view of equipment health, system performance and immediate maintenance priorities.

Key use cases and real-world impact

By converting real-time building data into actionable insights, predictive maintenance delivers measurable results across four core use cases.

24/7 equipment performance monitoring

OpenBlue Equipment Performance centralizes equipment health status and performance trends through continuous monitoring of more than 130 building data sources. AI-powered fault alerts and recommendations help teams identify performance gaps, emerging equipment issues and cost-reduction opportunities before they develop into larger operational problems. This visibility can reduce downtime and help critical departments maintain continuous operations.

Children’s of Alabama implemented OpenBlue Central Utility Plant Optimization across five major buildings. Combined with infrastructure upgrades and new controls, the system helped reduce unexpected repairs and system downtime while improving the reliability of hot water and cooling for critical hospital spaces. This ultimately reduced natural gas use by 69% and delivered $870,000 in annual cost savings ($170,000 directly attributed to OpenBlue).

AI-powered fault detection and diagnostics

Automated fault detection and diagnostics identify suboptimal conditions affecting equipment performance and energy use. AI-generated recommendations can help teams investigate issues earlier, while integrated workflows support a more closed-loop maintenance process.

A major healthcare institution with over 30 operating rooms struggled to manage temperature, humidity and pressure due to limited real-time visibility. By installing OpenBlue in two operating rooms, they connected occupancy sensors, surgical schedules and digital displays to automatically adjust environmental controls based on room usage.

Automated HVAC adjustments cut energy waste in unoccupied rooms and delivered $5,000 in annual savings per OR. Meanwhile, cloud-based trend reporting improved system visibility and compliance without disrupting clinical workflows.

Alarm management with prioritization and routing

OpenBlue Equipment Performance manages the ingestion, prioritization, fault monetization and routing of building management system and equipment alarms. By filtering lower-priority noise, the system reduces alarm fatigue and directs attention toward conditions that require immediate action. This gives technicians clearer visibility into urgent issues without overwhelming them with disconnected alerts.

Unified and remote command center

A unified operating center provides a single-view dashboard across building assets, helping facility teams respond with full system context. Remote visibility enables teams to assess conditions across departments, allocate maintenance resources and coordinate incident response from one interface.

Moving from reactive chaos to predictive resilience

Shifting from reactive firefighting and calendar-based servicing to predictive maintenance provides a stronger foundation for 24/7 healthcare operations.

By combining continuous monitoring, AI fault detection, prioritized alarms and centralized management with OpenBlue, facilities move from manually juggling competing building demands to relying on coordinated intelligence that protects mission-critical patient care.

Turn healthcare facility data into actionable insights that improve resilience

See OpenBlue for healthcare

Frequently asked questions

  • How does predictive maintenance differ from traditional preventive maintenance in a hospital setting?
    Traditional preventive maintenance relies on fixed service intervals, regardless of actual equipment condition or use. Predictive maintenance uses real-time performance data, fault detection and equipment trends to identify degradation earlier and help teams intervene at a more appropriate time. In hospitals, this can reduce unnecessary servicing while lowering the risk of failures that affect critical clinical spaces.
  • How does OpenBlue integrate with our existing building management systems and maintenance workflows?
    OpenBlue is designed to connect with existing building management systems, equipment data sources and computerized maintenance management systems. It can centralize equipment information, prioritize alarms, surface diagnostic recommendations and support automated work-order creation. This allows facility teams to add a unified intelligence layer without replacing every existing building system.
  • What is the ROI of implementing predictive maintenance in a healthcare facility?
    ROI can include reduced downtime, fewer emergency repairs, longer equipment lifecycles, lower energy use and less time spent on manual monitoring and troubleshooting. Healthcare organizations may also benefit from stronger compliance documentation, faster response times and fewer disruptions to revenue-generating clinical spaces.