Highlights:

  • Healthcare facility teams are under pressure to maintain safe, compliant critical environments while managing labor shortages, aging infrastructure and rising energy costs
  • Operating rooms are among the most energy-intensive spaces in a hospital, but many still run at full “ready” conditions even when they are unused
  • OpenBlue digital solutions help healthcare organizations connect building data, clinical schedules and compliance workflows so complexity becomes easier to manage


The pressure on healthcare facilities is not easing

Healthcare facility teams are being asked to do four hard things at once: keep critical environments safe, prove compliance on demand, reduce energy waste and manage it all with fewer skilled workers. Together, these challenges create a systems-level problem that cannot be solved through manual processes alone.

During a recent Johnson Controls healthcare webinar with facility leaders, participants were asked what is driving complexity in critical environments such as operating rooms and isolation rooms. The leading response was labor shortages, cited by 71% of participants. Other pressures included regulatory compliance, alarm fatigue and disparate systems that create a lot of data but not enough insight.

The opportunity is to stop treating complexity as something teams must manually absorb. With the right digital foundation, healthcare organizations can turn building data into better visibility, faster decisions and stronger operational resilience.

Why critical environments are difficult to manage

Operating rooms, airborne infection isolation rooms and other critical spaces carry higher stakes than typical building areas. They must maintain specific conditions for temperature, humidity, pressure and ventilation while supporting unpredictable clinical workflows.

ASHRAE 170 provides ventilation guidance for healthcare facilities, including requirements for air changes, pressure relationships and environmental conditions in critical spaces. ASHRAE 90.1 addresses energy performance and now includes stronger language around reducing airflow during unoccupied periods in spaces such as operating rooms.

That creates a constant tradeoff:

  • Run too low, and the room may fall out of compliance or take too long to recover before a procedure
  • Run too high, and the facility wastes energy and may weaken ventilation effectiveness
  • Rely on manual processes, and teams spend too much time documenting conditions instead of managing risk

Operating rooms show the challenge clearly. “If we look at some of these critical spaces like an OR, they’re typically another three to six times higher in energy use intensity within the hospital itself,” said Charlie Gans, Global Portfolio Leader for Healthy Buildings and Sustainability. But energy is only part of the problem. Many hospitals keep operating rooms at full conditions 24/7 because scaling back airflow raises valid concerns about recovery time, pressure control, temperature, humidity and room readiness.

Three ways digital solutions turn complexity into control

1. Connect building data to clinical workflows

Most healthcare facilities already collect the data they need. Building automation systems track temperature, humidity, pressure, airflow and equipment performance. The problem is that this data often sits inside engineering systems, while the clinical teams who depend on room readiness may not have clear visibility.

OpenBlue Operating Room Optimization helps close that gap by connecting building automation data with surgery schedules, occupancy sensors and staff-facing interfaces. When the operating room schedule changes, the building management system can adjust with it. If a room becomes occupied or a case runs long, occupancy data and manual override options add an extra layer of protection.

  • Scheduling integration aligns room conditioning with planned procedures.
  • Occupancy sensing helps account for late updates, emergencies and overruns.
  • Staff visibility gives clinical teams a simple way to see room status and take action when needed.

2. Reduce energy waste without compromising readiness

Many hospitals know they can save energy by reducing airflow in unused operating rooms. What holds them back is risk. If a room is suddenly needed, teams must be confident it can return to the correct temperature, humidity, pressure and ventilation conditions before care begins.

OpenBlue Operating Room Optimization addresses that risk by using automated mode switching. Rooms can move between full “ready” conditions and reduced “standby” conditions based on schedule data, occupancy and manual override. The result is a more disciplined energy strategy that does not depend on someone manually watching a schedule and changing control settings.

See how one healthcare institution used OpenBlue to save $5,000 annually per OR

Read the case study

3. Make compliance easier to prove

Compliance is not only about whether a room is in range at a single moment. “That’s one of the main things we see with Joint Commission: not only do they want to see, ‘Are you in the right parameters?’ but also, ‘Do you have the right processes in place?’” said Kyle Shamrock, Executive Director of Product Management for OpenBlue Industry Solutions and Connected Services. That means healthcare facilities need reliable records that show how critical environments performed over time.

OpenBlue Critical Environments Advisor supports this need by automating data collection and compliance reporting across critical spaces. Instead of relying on manual logs, teams can see whether rooms are within design parameters, identify excursions faster and generate reports that support audits and internal reviews.

The value is practical: fewer manual steps, better issue visibility and more confidence that critical spaces are ready when patients and clinicians need them.

From reactive facilities to smarter healthcare environments

The long-term goal is not simply to automate tasks. It is to help healthcare facilities move from reactive operations to smarter, more autonomous environments. In that model, building systems do more than collect data. They help interpret conditions, adjust operations and support the people responsible for patient care.

That shift matters because the next generation of healthcare operations will depend on resilience. Facility teams will need to manage stricter standards, leaner staffing models, more outpatient care and higher expectations for energy performance. The organizations that succeed will be the ones that can connect data to action quickly.

For healthcare leaders, the strategic advantage is clear: greater operational resilience, safer critical environments, less manual compliance work, lower energy waste and better visibility across the spaces that matter most. As Janice Howse, Industry Executive Director of Healthcare summarized, “It helps staff really focus on patient care while the buildings help focus on the things they need to. Digital and AI-driven solutions do create that strategic advantage.”

Turn healthcare complexity into control

Explore healthcare solutions

Frequently asked questions

  • What is OpenBlue Operating Room Optimization?
    OpenBlue Operating Room Optimization is a Johnson Controls digital solution that helps healthcare facilities reduce energy waste in operating rooms by connecting building automation systems with surgery schedules, occupancy sensing and staff override capabilities.
  • How does OpenBlue Critical Environments Advisor support compliance?
    OpenBlue Critical Environments Advisor helps automate the collection and reporting of critical environment data, including temperature, humidity, pressure and airflow. This gives facility teams a clearer view of room status and simplifies documentation for audits and internal reviews.
  • Why are operating rooms so energy-intensive?
    Operating rooms require high ventilation rates, precise pressure relationships and tightly controlled temperature and humidity. These conditions protect clinical readiness, but they can also drive energy use when rooms stay at full operating conditions while unoccupied.