Video: AI 101 webinar series

Part 3 on-demand

AI 101: AI under the hood

Discover why AI-powered building applications are only as effective as the data foundation behind them.

In Part 3 of the AI 101 Webinar Series, OpenBlue experts Sudhanshu Dixit and David Duncan explore how connected systems, harmonized data, and scalable digital infrastructure create the foundation for intelligent building operations. The conversation examines how building data is collected, standardized, and made accessible across different systems, vendors, and technologies.

Through practical examples and a conversational discussion of the underlying technology, viewers will learn how a connected data platform can support dashboards, integrations, automation, analytics, AI applications, and more responsive operational decision-making. The session also introduces capabilities such as automated onboarding and the OpenBlue Developer Portal, which help organizations access and use building data more effectively.

Speakers

Sudhanshu Head Shot

Sudhanshu Dixit

Lead Product Manager, OpenBlue Platform and Onboarding, Johnson Controls

David Dunkin Head Shot

David Duncan

Engineering Leader, OpenBlue, Johnson Controls

Key takeaways

Icon

AI-powered applications depend on connected, consistent, and usable building data.

JCI_Icons_Data_Blue-07

Building data often exists across different systems, vendors, generations, and protocols, making it difficult to use at scale.

JCI_Icons_Data_Blue-30

A connected data platform can standardize and normalize building data, creating a trusted foundation for analytics, automation, integrations, and AI.

JCI_Icons_Data_Blue-33

Open APIs and developer tools allow organizations to use building data in dashboards, enterprise applications, customized workflows, and other digital solutions.

JCI_Icons_Miscellaneous_Blue-08

Automated onboarding can reduce the time and manual effort required to connect and categorize building systems and data points.

  • Transcript summary

    AI 101 Webinar Series: Part 3

    AI Under the Hood: The Data & Technology Powering Intelligent Buildings

    Overview

    Part 3 of the AI 101 Webinar Series explored the technology and data foundation behind AI-powered building applications. Sudhanshu Dixit and David Duncan discussed how connected systems, harmonized data, and scalable digital infrastructure help organizations move beyond isolated information toward more intelligent building operations.

    The session emphasized a central theme: AI is only as effective as the data behind it. For organizations to successfully use AI, analytics, automation, or advanced reporting, building data must first be connected, standardized, accessible, and ready for use across the organization.

    The Building Data Challenge

    Most buildings contain equipment from multiple vendors, generations, and protocols. As a result, operational data is often fragmented across disconnected systems and may be structured or labeled differently depending on where it originated.

    This fragmentation can create several challenges:
    • Slow decision-making caused by disconnected data sources
    • Significant manual effort for reporting and data management
    • Limited visibility across buildings and real estate portfolios
    • Siloed operational, IT, and business systems
    • Difficulty scaling analytics, AI, and digital transformation initiatives

    Having large amounts of building data does not automatically create intelligence. The data must be organized, contextualized, and made available in a consistent format before it can effectively support AI applications or operational decision-making.

    Creating a Trusted Data Foundation

    The OpenBlue Data Platform helps connect building systems and data sources across different vendors and technologies. It standardizes and normalizes that information so teams and applications can work with consistent, usable data.

    By creating a connected and trusted data foundation, organizations can use building information to support:

    • Reporting and dashboards
    • Operational analytics
    • AI-powered applications
    • Automated workflows
    • Enterprise system integrations
    • Portfolio-wide visibility
    • Customer-developed applications and solutions

    This data foundation helps organizations move from managing isolated systems toward using building information more consistently across operations, IT, and business functions.

    From Raw Data to Building Intelligence

    Building systems continuously generate information about equipment operation, environmental conditions, occupancy, performance, and energy use. However, this information may come from different technologies and may not use consistent naming conventions or data structures.

    A data platform helps bring this information together and create a common structure that applications can understand. Once building data is connected and standardized, it becomes more useful for identifying patterns, developing dashboards, integrating systems, automating processes, and enabling AI-driven recommendations.

    Rather than creating separate integrations for every individual application, organizations can establish a common data foundation that supports multiple current and future use cases.

    Automated Onboarding

    One of the capabilities highlighted during the webinar was automated onboarding. This capability supports the automated discovery and categorization of devices and data points, reducing the manual work traditionally required to connect and organize building information.

    Automated onboarding can help organizations:

    • Discover connected equipment and data points
    • Categorize building information
    • Reduce manual data-mapping activities
    • Accelerate implementation
    • Scale deployments across larger campuses and portfolios

    The sales activation guide created for the webinar states that implementation time can be reduced by up to 95%, allowing some large campus deployments to move from months to days.

    OpenBlue Developer Portal

    The session also introduced the OpenBlue Developer Portal, which gives customers and partners access to APIs, documentation, and a development environment.

    These capabilities allow organizations to use their building data in ways that support their specific business and operational requirements, including:

    • Creating customized dashboards
    • Developing applications
    • Connecting building data with enterprise systems
    • Building automated workflows
    • Supporting AI and analytics initiatives
    • Creating integrations and tailored user experiences

    The Developer Portal provides access to the same underlying platform that supports OpenBlue solutions, while giving customers and partners additional flexibility to develop their own use cases.

    Supporting Existing Building Environments

    Organizations do not necessarily need to replace all existing equipment to begin creating a connected data foundation. OpenBlue is designed to work with building environments containing a mix of systems, vendors, and protocols.

    This approach allows organizations to focus on making existing building data more accessible and usable while developing a longer-term digital transformation strategy.

    Business and Operational Outcomes

    A connected data foundation can help organizations:

    • Accelerate access to operational insights
    • Reduce reporting and implementation effort
    • Improve confidence in building performance data
    • Increase visibility across buildings and portfolios
    • Integrate operational data with existing enterprise systems
    • Scale AI and analytics initiatives more effectively

    The broader value is not limited to AI. The same data foundation can support reporting, dashboards, portfolio visibility, integrations, workflows, and custom applications. AI becomes one of several use cases enabled by more accessible and consistent building data.

    Final Takeaway

    The webinar demonstrated that intelligent building outcomes do not begin with an individual dashboard, algorithm, or AI application. They begin with a strong data foundation.

    By connecting and standardizing information across building systems, organizations can create a scalable foundation for analytics, integrations, automation, and AI. This makes it easier to transform building data into useful insights and develop intelligent applications that support evolving operational and business needs.