How OpenBlue turns building data into energy-saving action with AI
Highlights:
- OpenBlue Intelligence harmonizes building data so AI can analyze energy, equipment and fault information in context.
- A conversational AI agent lets users ask natural-language questions and receive relevant insights, diagnostics and recommended actions.
- AI-driven optimization can move teams beyond finding problems to continuously adjusting equipment for better performance.
Buildings produce millions of data points, but more data does not automatically create better decisions. Facility teams still lose time moving between dashboards, interpreting disconnected signals and deciding which issue deserves attention first.
OpenBlue Intelligence addresses this widening gap. Built on an open, unified data platform, it harmonizes information from building systems and applies AI-powered applications, intelligent automation and autonomous performance capabilities. The result is a clearer path from raw data to prioritized action.
What does AI-driven building performance look like in practice?
Two customer examples show the progression from visibility to action: first, uncovering avoidable energy waste across a complex building and second, using predictive optimization to adjust a central plant throughout the day.
A London skyscraper uncovers £32,000 in potential energy savings
An iconic London skyscraper needed better visibility into pumps, boilers, air handling units and fan coil units to reduce energy waste and make progress toward its net zero commitments. A pilot across three floors brought equipment data together through Metasys and OpenBlue. The analysis identified inefficiencies, refined equipment schedules and highlighted smarter operating strategies, uncovering £32,000 in potential energy savings.
The value was not another dashboard. It was the ability to connect equipment behavior with energy performance, isolate opportunities and give operators a practical basis for action. The pilot also created a repeatable model that could be scaled across the tower.
A Las Vegas megaresort predicts demand and optimizes every 15 minutes
One of the largest resorts on the Las Vegas Strip relied on a labor-intensive legacy building automation system to manage a large chilled water plant. Operators had to react manually to changes in weather and occupancy.
Johnson Controls replaced the legacy system with Metasys and OpenBlue. AI-driven supervisory control in OpenBlue predicts chilled water loads, evaluates equipment combinations and makes efficiency adjustments every 15 minutes. These ongoing adjustments in “Auto Mode” resulted in $110,000 in annual utility cost savings and a 10.2% annual reduction in energy use.
This example shows the next step in the AI journey: moving beyond simply generating insights to using predictive models and automation to optimize chiller staging, pump speeds and cooling tower operations as conditions change.
See how OpenBlue Intelligence can make your building more efficient and resilient
How does OpenBlue AI turn complex data into clear action?
OpenBlue Intelligence supports facility teams’ AI workflows through four connected capabilities:
- Harmonize the data: OpenBlue brings information from energy, equipment, faults and other building systems into a unified data foundation. This common context helps the AI interpret relationships across systems instead of treating each signal in isolation.
- Understand natural-language questions: OBI, the OpenBlue conversational AI agent, allows users to ask questions about energy consumption, faults and equipment in everyday language. Teams can retrieve insights without navigating multiple applications or building custom reports.
- Synthesize findings and recommend actions: AI analyzes performance trends and anomalies, then surfaces concise insights, diagnostics and recommendations. This helps teams understand what is happening, why it matters and what to prioritize.
- Optimize and automate: For supported applications, AI-driven controls can act on the analysis. OpenBlue can adjust system performance in real time, automate workflows and support continuous improvement rather than one-time troubleshooting.
What makes the OpenBlue approach different?
Many tools add AI to a single dashboard or isolated feature. OpenBlue Intelligence applies AI across a connected building-data foundation and combines three differentiators:
- Building-ready context: harmonized data connects energy, equipment and fault information across a portfolio
- Operator-focused interaction: a conversational interface turns natural-language questions into relevant building insights and recommendations
- A path from insight to autonomy: AI-powered applications can support diagnosis, optimization and automated action on the same platform
Insight alone does not save energy. Teams need trusted context, a clear recommendation and a practical way to act. OpenBlue connects those steps so facility professionals can spend less time assembling information and more time improving performance.
See OpenBlue AI in action
Frequently asked questions
-
What is OpenBlue Intelligence?OpenBlue Intelligence is the AI layer within OpenBlue. It uses a unified building-data platform, AI-powered applications, intelligent automation and conversational experiences to help users improve building performance.
-
How does the OpenBlue conversational AI agent help facility teams?Users can ask natural-language questions about energy, equipment and faults. The agent retrieves relevant data and provides insights, diagnostics and recommended actions through one interface.
-
How can OpenBlue AI improve energy efficiency?OpenBlue AI can identify inefficient operating patterns, prioritize recommended actions and, in supported applications, optimize equipment automatically as building conditions change.
-
Does OpenBlue AI replace facility professionals?No. It reduces the manual work required to find, interpret and prioritize information. Facility professionals remain responsible for operational decisions while gaining faster access to actionable building intelligence.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)