Direct answer

Building decarbonization is the process of reducing or eliminating greenhouse gas emissions from the energy used to operate a commercial building — including heating, cooling, lighting and plug loads. For facility managers, it means identifying emissions across Scope 1, Scope 2 and Scope 3, improving energy efficiency and shifting building systems away from fossil fuels.

Key takeaways

  • Building decarbonization means reducing the GHG emissions associated with operating a building through energy efficiency and reduced reliance on fossil fuels
  • Scope 1 covers direct emissions, Scope 2 covers emissions associated with purchased energy and Scope 3 covers value-chain emissions outside a facility manager’s direct control
  • Thermal efficiency and electrification reduce operational emissions by lowering energy demand and shifting building systems away from fossil fuels
  • Building performance standards, refrigerant regulations and economic pressures are influencing the timing and priorities of decarbonization projects
  • Facility managers can build a decarbonization pathway by establishing a baseline, identifying emissions sources and aligning improvements with capital cycles and compliance deadlines

Facility teams already manage energy costs and equipment performance as part of keeping buildings running efficiently. Decarbonization extends that work by focusing on how building improvements can reduce emissions as well as energy use.

Many facility teams already have the raw materials for a decarbonization plan: utility bills, equipment inventories and capital schedules. The challenge is turning them into a clear view of emissions and a practical order of action.

Explore the core terminology and regulatory drivers of building decarbonization and discover a practical framework for prioritizing and planning improvements in commercial buildings.

What decarbonization means in a commercial building context

Building decarbonization means reducing the greenhouse gas (GHG) emissions associated with operating a commercial building. These emissions include carbon dioxide released when fossil fuels such as natural gas are burned for heating, as well as emissions associated with the electricity a building uses.

Decarbonization involves improving energy efficiency and shifting building systems toward lower-carbon energy sources. Operational carbon comes from the energy used to run a building, while embodied carbon is associated with its construction and building materials.

For facility managers, decarbonization is the next evolution of the energy efficiency work they already manage. The focus expands from reducing energy use and costs to reducing the resulting emissions.

Scope 1, 2 and 3 emissions: What facility managers need to know

A building’s carbon footprint is the total GHG emissions associated with it. These emissions are grouped into three scopes based on where they originate and whether they come from sources the organization owns or controls, purchased energy or other activities in its value chain.

Scope 1: Direct emissions

Scope 1 covers direct emissions from sources the organization owns or controls. In buildings, these sources can include natural gas burned in boilers, diesel used in backup generators and refrigerant leaks from HVAC equipment.

Scope 2: Indirect energy emissions

Scope 2 covers emissions associated with purchased electricity, steam, heating and cooling. The carbon intensity of the local power grid affects how much carbon a building’s electricity use generates. A building drawing electricity from a grid that relies heavily on coal and natural gas can generate more emissions than an equally energy-efficient building on a grid powered by renewable or other low-carbon energy sources.

Scope 3: Value-chain emissions

Scope 3 incorporates emissions from sources where facility managers have influence, but not direct control. These include tenant energy use, commuting, waste and procurement. Tracking these emissions helps facility managers identify opportunities to influence reductions. It can also support organizations preparing for expanded value-chain reporting, including those subject to California's Climate Corporate Data Accountability Act (SB 253) Scope 3 reporting requirements beginning in 2027.

Electrification and thermal efficiency are the two key decarbonization levers

Reducing operational emissions requires lowering a building’s energy demand and shifting away from fossil fuels.

  • Facility electrification replaces fossil-fuel-powered equipment with electric alternatives that can run on lower-carbon electricity.
  • Thermal efficiency reduces the amount of energy needed for heating and cooling through envelope improvements, heat recovery and smarter controls.

Reducing heating and cooling demand means electrified systems have less work to do, making the transition to electricity more efficient while reducing the building’s carbon emissions.

Regulatory and economic drivers shaping the timeline

Facility managers must understand the primary regulatory and economic factors prompting commercial buildings to lower their carbon footprint.

Cities across the US are adopting building performance standards that can set energy or emissions limits for covered buildings. NYC Local Law 97, for example, sets emissions limits for many large buildings and includes financial penalties for noncompliance. Additional limits take effect in 2030.

Federal refrigerant regulations affect decarbonization as well. The American Innovation and Manufacturing Act of 2020 (AIM Act) is phasing down hydrofluorocarbons (HFCs), a type of refrigerant. Many HFCs have a high global warming potential, so reducing their production and use can lower refrigerant-related emissions. The law also restricts certain HFCs in new HVAC and refrigeration equipment.

Federal tax incentives can help offset the cost of qualifying energy-efficiency projects, although available incentives and eligibility requirements are changing. Before including incentives in a project plan, confirm current eligibility, construction-start rules and documentation requirements with a qualified tax adviser.

Finally, economic pressures are strengthening the business case for decarbonization. Rising energy costs can increase operating expenses, while tenant and investor expectations around environmental, social and governance (ESG) issues can influence leasing, access to capital and asset value.

How to begin mapping your building’s decarbonization pathway

To ensure decarbonization efforts deliver lasting value and long-term regulatory compliance, facility owners and managers can follow a structured, step-by-step approach to evaluating buildings:

  1. Establish an energy and emissions baseline. Audit utility bills, fuel consumption records and equipment inventories to quantify current Scope 1 and Scope 2 emissions. Tools like ENERGY STAR® Portfolio Manager® can help benchmark performance against comparable buildings.
  2. Identify and classify emission sources by scope. Map each source to its Scope 1, 2 or 3 category. This converts a general energy audit into a clear view of where emissions come from.
  3. Prioritize load reduction before equipment replacement. Reduce heating, cooling and plug loads through envelope improvements and lighting upgrades so any new equipment can be right-sized.
  4. Evaluate electrification opportunities by system. Identify fossil-fuel equipment that can be replaced with electric alternatives. Prioritize equipment nearing end of life to align upgrades with decarbonization goals.
  5. Schedule improvements against compliance deadlines and capital cycles. Map planned improvements to regulatory deadlines and existing capital plans. This creates a phased roadmap that helps avoid compliance penalties and prevent retiring equipment before the end of its useful life.
  6. Monitor performance and adjust over time. Use available building and utility data to track energy use and emissions, verify the effect of completed projects and identify new opportunities for improvement.

A unified building platform that aggregates real-time operational data across systems allows facility managers to continuously track Scope 1 and Scope 2 emissions, predict energy loads and automate efficiency adjustments. This can help teams track decarbonization progress, identify unexpected changes in energy use and maintain records for reporting.

Decarbonization is the next evolution

Decarbonization isn’t a new mandate imposed on facility teams. It formalizes the efficiency and performance optimization work they already do.

A practical decarbonization plan starts with three things: a reliable baseline, a clear map of emissions sources and a schedule tied to equipment replacement and regulatory deadlines.

Facility teams do not need to solve everything at once. They need enough information to choose the right next step.

Learn how connected building data can support your decarbonization strategy

Explore OpenBlue Net Zero

Frequently asked questions

  • What is the difference between Scope 1 and Scope 2 emissions?
    Scope 1 covers direct emissions from sources a building controls, such as natural gas burned in boilers, diesel used in backup generators and refrigerant leaks. Scope 2 covers indirect emissions associated with purchased electricity, steam, heating and cooling.
  • What does electrification mean for an existing building?
    Electrification means replacing equipment that burns fossil fuels with electric alternatives. In an existing building, this could include replacing a gas-fired heating system with electric heat pumps as equipment reaches the end of its useful life.
  • Which regulations require building decarbonization?
    Requirements vary by location. Building performance standards such as NYC Local Law 97 set emissions limits for covered buildings, while other federal, state and local rules affect specific aspects of decarbonization. For example, the federal AIM Act phases down HFC refrigerants and restricts high-global-warming-potential HFCs in new HVAC and refrigeration equipment.